The problem is not with the load module that you are programming, it is with the modules that are not being programming. The list length (or points) applies to the entire load mainframe, so the default number of points on the other load modules (or channels) is what is causing the error.
Try setting the number of list points on other load modules in the mainframe to a lower number.
Applies to: N3300A, N3301A, N3302A, N3303A, N3304A, N3305A, N3306A, N3307A
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |